How to run initialization script when connect to target through JTAG RCW override

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to run initialization script when connect to target through JTAG RCW override

1,706 Views
henryeng
Contributor I

Hello

 

I am trying to bring up a new board based on the T1020.  I have connected to the target using code warrior JTAG RCW override.  When I connect to the target this way, code warrior does not give me the option to initialize the cpu (I want to use a modified T1020RDB_core.tcl configured for our target to burn the RCW into NAND flash).  Is there a way to do this?  Note.  The target board is to use the Hard coded RCW (with this method, the initialization option is avail)

 

Thanks

Henry Eng

Labels (1)
0 Kudos
Reply
1 Reply

1,437 Views
addiyi
NXP Employee
NXP Employee

After you select the jtag_chain file as Target Type, you can add the init file as in below image:

pastedImage_0.png

Adrian

0 Kudos
Reply