How to output the Fresscale building result output to the log.txt through file redirection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to output the Fresscale building result output to the log.txt through file redirection

791 次查看
kevinding
Contributor I

Hello community:

       When I use the GUI interface, click "Make" button,I can get the target project file Project.abs.s19. For using computer resources effectively we don't want to use the GUI. Now we using command "set CmdIDE_PATH="C:\Program Files (x86)\Freescale\CWS12v5.1\bin\CmdIDE.exe"  /r /b /c Project.mcp > log.txt" , after that operation, we can get a dos window output such as 捕获1.PNG

content of log.txt is "Freescale CodeWarrior IDE. Hit /? for help"

in this case, building is pass, but I cannot output the "No Error.<Code 0>" to the log.txt file through a file redirection.  So How I can get "No Error.<code 0>" to the log.txt, thank you.

0 项奖励
回复
1 回复

723 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Kevin.

Please refer my answer here

https://community.nxp.com/thread/458622 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复