How to make Library using CW2.10(for MPC56XX)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to make Library using CW2.10(for MPC56XX)

ソリューションへジャンプ
4,444件の閲覧回数
Luke_Chun
NXP Employee
NXP Employee

Dear Team

 

May I ask about the CW2.10 for MPC56XX?

 

How to make Library using CW2.10(for MPC56XX)?

I tried to follow using S08 or S12's community guidance but it is not working for CW2.10.

I think that I took some mistake but I did not find the root cause.

I wish to find some reference / example for it.

 

Thank you.

 

0 件の賞賛
返信
1 解決策
4,437件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Luke,

If you want to generate a library, please create the project for library by File->New-> Empty Project. Then open Target Settings by 'ALT'+'F7' key and set the linker as 'PowerPC EABI' on 'Target Settings' panel. Also change the 'Project Type' as 'Library' on the 'EPPC Target' panel and type the name for output library.

You can refer to the projects under the directory below. These projects are used to generate runtime libraries for MPC5:

c:\Program Files (x86)\Freescale\CW for MPC55xx and MPC56xx 2.10\PowerPC_EABI_Support\Runtime\Project\

Regards

Lukas

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,438件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Luke,

If you want to generate a library, please create the project for library by File->New-> Empty Project. Then open Target Settings by 'ALT'+'F7' key and set the linker as 'PowerPC EABI' on 'Target Settings' panel. Also change the 'Project Type' as 'Library' on the 'EPPC Target' panel and type the name for output library.

You can refer to the projects under the directory below. These projects are used to generate runtime libraries for MPC5:

c:\Program Files (x86)\Freescale\CW for MPC55xx and MPC56xx 2.10\PowerPC_EABI_Support\Runtime\Project\

Regards

Lukas

 

0 件の賞賛
返信
4,428件の閲覧回数
Luke_Chun
NXP Employee
NXP Employee

Hello Lukas

 

Thanks for your reply.

May I ask one more question?

 

I made Library but I have one more question.

 

I wish to locate the dedicated area about Library.

I tried to use some pragma function like below.

The function of same code file is possible to locate on my dedicated area.

However, the library function is not located on my dedicated area.

 

 

 

for your understanding, I have attached project...

I wish to locate the function and library into 0x31000.

Luke_Chun_3-1666147134585.png

 

I tried to do like below.

Luke_Chun_0-1666146739892.png

 

 

However, only function of same file is located on 0x31000...

Luke_Chun_1-1666146840622.png

Luke_Chun_2-1666147107598.png

 

how to locate the library into 0x31000?

 

Thank you.

 

 

 

 

0 件の賞賛
返信
4,411件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Luke,

I found quick solution in AN4497:

lukaszadrapa_0-1666334656797.png

 

I did quick test in your project, so I added this to the linker file:

GROUP : {
.libcode (VLECODE) LOAD (0x00031000) : {
test.a (.text)
}
.libconst:
{
test.a (.rodata)
}
} > CCPBL_HAE_SECURITY_LIBRARY_Section

And here's the result:

lukaszadrapa_1-1666334773060.png

Regards

Lukas

4,401件の閲覧回数
Luke_Chun
NXP Employee
NXP Employee

Hi Lukas

 

Thanks for your support.

It is correct what I am needed!!

 

Thank you.

0 件の賞賛
返信