How to create and flash the boot image for baremetal application in code warrior for T2081?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to create and flash the boot image for baremetal application in code warrior for T2081?

6,649 Views
Vimalprasad
Contributor II

I have created a bareboard hello world application in the CodeWarrior for T2081 processor.

I can able to debug the application and i want to flash the application.

 

Is this RCW needed for the bareboard application to flash and boot?

Could you please provide the procedure for creating boot image(boot.bin) and flashing the bareboard application on the T2081 processor?

0 Kudos
Reply
9 Replies

6,611 Views
yipingwang
NXP TechSupport
NXP TechSupport

1. Configure the CodeWarrior as ROM version and build this project.

2. Please use the following command to convert the ELF file to bin file.

C:\Users\nxa22585>C:\Freescale\CW_PA_v10.5.1\Cross_Tools\gcc-4.9.2-Ee6500-aeabi\bin\powerpc-aeabi-objcopy.exe -O binary -S C:\Users\nxa22585\Downloads\t2080rdb\t2081-core00\ROM\t2081-core00.elf C:\Users\nxa22585\Downloads\t2080rdb\t2081-core00\ROM\test.bin 

3. Please refer to T2081QDS_gcc-aeabi_ROM.lcf to deploy the test.bin file at 0xEFF00000  on NOR flash.

You need to program RCW on the target board first.

For flash programming, please refer to https://community.nxp.com/t5/CodeWarrior-Development-Tools/Flash-Programmer-for-CodeWarrior-Power-Ar...

 

0 Kudos
Reply

6,548 Views
Vimalprasad
Contributor II

Hi @yipingwang ,

Currently I'm working on the T2080RDB,I have created the ROM version of the project and created the boot.bin file with using the mentioned command.

I have flashed the PBL.bin at the starting address 0xE0000000 and the boot.bin file in the 0xE7F00000 where my unprotected region of my NOR flash is 0xE0000000 to 0xE7FFFFFF and the protected region is 0xE8000000 to 0xEFFFFFFF.

After that I can able to flash but the booting is not happening.

I have created the ROM version of the project in the codewarrior , while debugging the project it not stopping in the main function.
Can you tell me how to debug the ROM version for the codewarrior?

I have done the modification in the T2080RDB-PCIe_gcc-aeabi_ROM.lcf . I have attached the lcf file with the modification have some errors mentioned in the screenshot.

Can you tell me any other configuration have to do for the booting have happen?

lcf_error.pnglcf_error.png

0 Kudos
Reply

6,435 Views
Vimalprasad
Contributor II
Can you please provide the solution for the above queries?
0 Kudos
Reply

6,425 Views
yipingwang
NXP TechSupport
NXP TechSupport

What is the size of your binary file?

What address did your program it at?

0 Kudos
Reply

6,415 Views
Vimalprasad
Contributor II
I'm programming PBL (PBL.bin) at 0xE0000000 having size of 1KB.
I'm programming the binary file(boot.bin) at 0xE7F0000 having size of 1024KB
0 Kudos
Reply

6,374 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please define lcf file as the following, and program the bin file at 0xEFF00000.

/* Default linker script, for normal executables */
OUTPUT_FORMAT("elf32-powerpc", "elf32-powerpc",
      "elf32-powerpc")
OUTPUT_ARCH(powerpc:common)
ENTRY(__start)
MEMORY {
ram    : org = 0x00002000, l = 0x7FFFFFFF
rom   : org = 0xEFF10000, l = 0x000EEFFF
}
 
SECTIONS
{
 
  _stack_addr = 0x003dfff0;
  _stack_end  = 0x003d7ff0;
  
  _heap_addr  = 0x3cfff0;
  _heap_end   = 0x3d7ff0;
 
  .intvec 0xEFF00000 :
  {
    *(.intvec)
  } = 0xffff
  
  .reset 0xEFFFFFFC :
  {
    *(.reset)
  } = 0x4
 
  .init 0xEFFFF000 :
  {
    *(.init)
    *(.init_data)
  } = 0xFFC
  
0 Kudos
Reply

6,575 Views
Vimalprasad
Contributor II

Hi @yipingwang , thanks for your response.

In my nor flash the address start from the 0xE0000000 to 0xE7FFFFFF is in unprotected and the address from 0xE8000000 to 0xEFFFFFFF is in protected mode.

I have tried to flash in 0xEFF00000 , it showing write protected error, flash not happened.

So, I flashed at 0xE7F00000 but the booting is not happening. 

Where I have to flash my boot.bin file so that it can boot?

In this T2081QDS_gcc-aeabi_ROM.lcf file any modification have to do , can you tell the modifications?

 

0 Kudos
Reply

6,461 Views
yipingwang
NXP TechSupport
NXP TechSupport

bootloader image should be deployed at the end of the NOR flash.

0 Kudos
Reply

6,433 Views
Vimalprasad
Contributor II
Thanks for your response,
I had flashed the boot image at the end of the NOR flash, then also I cannot see the boot prints.
0 Kudos
Reply