How to change the workspace name of CodeWarrior(V10.5)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to change the workspace name of CodeWarrior(V10.5)?

跳至解决方案
3,303 次查看
PeterTsai
Contributor II

I have built a project in workspace. and I rename the workspace(directory) name. then open the new workspace name. but it show "Invalid workspace in use" message. May I rename the worksapce name?

 

Peter Tsai

标签 (1)
1 解答
2,526 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Peter

A workaround is to copy the old workspace folder, then name the new folder and delete the “.metadata” subfolder under it.

The open CodeWarrior v10.5, and click on <File> menu->Switch Workspace to select the new folder.

But you need to drag the project or import in to the CodeWarrior Project view. The old project view is not kept.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,527 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Peter

A workaround is to copy the old workspace folder, then name the new folder and delete the “.metadata” subfolder under it.

The open CodeWarrior v10.5, and click on <File> menu->Switch Workspace to select the new folder.

But you need to drag the project or import in to the CodeWarrior Project view. The old project view is not kept.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------