How to change the static_code path when the project opened by others

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to change the static_code path when the project opened by others

跳至解决方案
2,702 次查看
jason_zhang
Contributor III

Hi, I sent my codewarrior 10.6.4 project(buit by PE) to my colleague, the static_code file can not be found when she opened it.

The path is wrong, it's still point to my workspace.

How to change the static_code path when the project opened by my colleague.

 

132848_132848.JPG打不开文件错误.JPG

 

Thank you.

Jason

标签 (1)
0 项奖励
回复
1 解答
2,595 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jason,

Static_Code is defined at Processor Expert Project  Option settings:

pastedImage_0.png

please check if your project is as same as my highlight screenshot.

with above setting, normally processor expert project can identify Static_Code folder well. if it's not on your side. I suggest you:

1. do menu "project", "Clean...".

2. click icon of regenerating processor expert code:

pastedImage_1.png

3. rebuild project. how does it work?

if above suggestion can not work for you, add Static_Code path to project properties:

pastedImage_2.png

can this help you work out the problem?

if not, please sent your project to me, I will look into the problem directly. thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,596 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jason,

Static_Code is defined at Processor Expert Project  Option settings:

pastedImage_0.png

please check if your project is as same as my highlight screenshot.

with above setting, normally processor expert project can identify Static_Code folder well. if it's not on your side. I suggest you:

1. do menu "project", "Clean...".

2. click icon of regenerating processor expert code:

pastedImage_1.png

3. rebuild project. how does it work?

if above suggestion can not work for you, add Static_Code path to project properties:

pastedImage_2.png

can this help you work out the problem?

if not, please sent your project to me, I will look into the problem directly. thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,595 次查看
jason_zhang
Contributor III

Hi Jenny

Thank you for your help. It works when my colleague did it as follow

2.click icon of regenerating processor expert code

Thank you very much!

Jason

0 项奖励
回复
2,595 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome!


Have a great day,
Jennie Zhang

0 项奖励
回复