How to change framesize correctly ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change framesize correctly ?

1,234 Views
wolfgangschwab
Contributor I

Hello guys,

 

in order to read data with SPI I have to read with 18 clocks(data sheet ADC). The default framesize is 1 byte. If I read 3 times the problem is a pause between each byte. This probably causes errors.

Here is the code I wrote so far:

 

uint_32 frame = 24;

_io_ioctl(spi, IO_IOCTL_SPI_SET_FRAMESIZE, &frame);

_io_read(spi, &buffer, 1);

 

This doesnt work because the clock only sends one pulse and data can not be read.

If I change it to

_io_read(spi, &buffer, 24);

I get 24 pulses but no data on my MISO.

I'd be thankful for advice

Labels (1)
Tags (2)
0 Kudos
Reply
0 Replies