How do I use gdb to control the CWTAP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I use gdb to control the CWTAP?

1,340 Views
jeffhodges
Contributor I

I ordered the CWTAP to send gdb commands to my target system.  I could not find any documentation on using gdb with the CWTAP; however, there is a nice video online showing that this is the intended design.  How do I send commands from my (gdb) shell to the CWTAP?

 

I've connected my host computer to the CWTAP which I've assigned a static IP of 192.168.1.2.  I can ping the CWTAP, so I have a valid IP connection. The CWTAP manual states that gdb uses port 2345.

 

From the (gdb) shell I tried the command:

(gdb) target remote 192.168.1.2:2345

 

However there was no response and the command timed out.

Labels (1)
0 Kudos
Reply
1 Reply

1,252 Views
addiyi
NXP Employee
NXP Employee

CWTAP doesn't include a gdb server that allow you to control the board. Communication with CWTAP is done using ccs. Starting with CodeWarrior for ARMv8, gdb connection is possible but only using gta, which know to "transform" gdb commands to ccs commands. 

There was an intention to move the gdb sevrer on CWTAP, but the project is obsolete. 

Adrian

0 Kudos
Reply