How could I put code into a freescale chip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How could I put code into a freescale chip

2,477件の閲覧回数
slanfys
Contributor I

Hello

Long story short I'm working with Codewarrior IDE and I have already a code ready to flash into a chip. The problem I badly have to be solved is that I am not able to flash de chip in which it is connected to my pc.

This case is so urgent and  I'm looking for someone who wants to share a while dealing this problem on skype, discord, facebook, etc, to solve this issue. I would also thank suggestions here

I appreciate and thank any kind of help.

0 件の賞賛
返信
3 返答(返信)

2,364件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Kot,

To solve your problem, please let us know:

1. what's your chip part number?

2. what's your debug interface?

3. do you have entire project code or only burning file(for example .s19 file)?


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,364件の閲覧回数
slanfys
Contributor I

1. MC9S08QE32

2. don't know what you mean

3. I have my entire project

0 件の賞賛
返信

2,364件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

>>2. don't know what you mean

I mean what emulator you are using for debug. BDM Multilink or ? If you don't know, please post its photos here.

You have entire project, you can burn code to chip flash with launch project debugger. when you click on debug button, and successfully launch debugger, the code is downloaded to chip.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信