Hi,
You must install CW for MCU v10.5 and MQX V4.0.2 (these are the last versions).
Under MQX installation, please have a look to:
- the folder \Freescale_MQX_4_0_2\doc\tools\cw -> the manual FSL_MQX_in_CW_10_x.pdf,
- the folder \Freescale_MQX_4_0_2\doc -> FSL_MQX_release_notes.pdf
the user_config.h will allow you to enable or not the BSP functions.
++++++++++++++++
extract of Manual
SPI I/O Driver
This driver supports the operation master mode. If enabled in user configuration, the SPI device drivers are installed during the BSP startup code as “spi0:” (or “spiX:” where X is index of the SPI module used). The SPI driver is significantly rewritten in the MQX 4.0, so that there is no distinct interrupt or polled driver type. See I/O User Guide for details. On Kinetis and Vybrid platforms, the driver uses DMA to function.
++++++++++++++++
There is an example for SPI ... under Basic example.
Regards
Pascal