How To use Backdoor key Security feature to make device secure and to get access by entering security key?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How To use Backdoor key Security feature to make device secure and to get access by entering security key?

2,544 次查看
Amit_Kumar1
Senior Contributor II

Hi

I am using Codewarrior 10.5 with PE 10.2. I want to make my kinetis uc secure and want to get access to it only if the 64 bit Backdoor key is matched. how to do this using PE? In PE there is a setting in which we can set all the required features for securing the device but my concern is how to use this feature? Using the following setting I have made my device secure by programming it using this settings , if I change the settings then also it programs. I considered it to ask for the security key or give some error so that I need to set the same settings to program the device, but that didn't happen. Please look into the matter. Thanks

 

11584_11584.jpgsecurity.jpg

 

Kind Regards

Amit Kumar

标签 (1)
0 项奖励
回复
1 回复

2,164 次查看
trytohelp
NXP Employee
NXP Employee

Hi Amit,

Personally I've never try this feature but I found some information about that.

Can you check the following :

            http://mcuoneclipse.com/2012/11/04/how-not-to-secure-my-microcontroller/

Other information:

Kinetis flash protection and security information:

      http://www.freescale.com/files/microcontrollers/doc/app_note/AN4507.pdf

      http://compass.freescale.net/livelink/livelink/230066320/Flash_security_and_protection.pptx?fu...

          


Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复