How Can I install CodeWarrior V6.3. on a Win7 64 bit computer?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How Can I install CodeWarrior V6.3. on a Win7 64 bit computer?

1,876 Views
jungwoojin
Contributor I

when i installed the CW v6.3, i can see the warning message about " CodeWarrior development studio for microcontrollers v6.3 is not compatible with Windows XP 64-bit installation."

 

 

Please tell me how to install the CW v6.3 in windows7 64bit.

 

Or, please tell the program to replace the CW v6.3.

 

MCU is 'S9S08AW16AMLD'

Labels (1)
0 Kudos
Reply
1 Reply

1,460 Views
trytohelp
NXP Employee
NXP Employee

Hi,

Please have a look to the message:

    Install CodeWarrior 6.3 Windows 7 & 10 x64 directly (Classic version)

Scroll down to have all information and option to install the CW for MCU v6.3 on Win 7 and higher version.


Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply