Help- using Integrated USB BDM of M52233Demo with CW10.5IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help- using Integrated USB BDM of M52233Demo with CW10.5IDE

1,475 次查看
pavanbg
Contributor I

Hello ,

 

I am using Codewarrior 10.5 Eclipse for MCUs on Win7 , I have a M52233Demo board and I want to use the Integrated USB BDM  with CW10.5 ,I have done the hardware jumper settings please help me with the configuration in CW10.5 .Thanks

 

Regards

Pavan

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,364 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

we were ever informed by P&E that BDM Modules are low cost BDM modules that are not intended to be used for anything else other than program the device present on the demoboard. Even attempting to program the same derivative part number but on an external target is not guaranteed it will work.  P&E does not support this and Freescale support should not assist customers who try to hack these boards to turn them into programmers.

hope this information can make sense for you.

----------------------------------------------------------------

this answer is for you. if this helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 项奖励
回复