Help about the USBTAP question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help about the USBTAP question

1,722 Views
_weh___george
Contributor I

I have programed one code with CodeWarrior V8.2,and I connect the USBTAP to PC. However,when I tried to debug the code,there is one question about the USBTAP protocal, described as"Unknown protocal error",so I try to load configuration of the USBTAP driver with the codewarrior connection server. But there may be some question called ERROR Config Syntax:balalala.........ps: I use a PC with windows x64 and I have solved the compatibility problem with the x86 windows complied with the official way. 

Therefor I need your help very much! Holy Crap! Where is my skill god! 

0 Kudos
Reply
0 Replies