Hello All, I want to program DSP56F805 for PMSM, can somebody guide me how to start ? which version of codewarrior is suitable?, I will be using windows7 operating system.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hello All, I want to program DSP56F805 for PMSM, can somebody guide me how to start ? which version of codewarrior is suitable?, I will be using windows7 operating system.

1,115件の閲覧回数
chandankumar
Contributor I

I am good at "python" programming but new to "C/C++". Kindly suggest me best way to start with it.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,044件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hi CHANDAN,

Please use CodeWarrior v8.3 to develop for DSP56F805, which can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC

It only supports C and assembly language.

CodeWarrior v8.3 can work on Windows 7. But to support USBTAP debugging on Windows 7, user needs to install the new CCS update, please search 'AN4338' on Freescale's website (www.freescale.com), and follow the instructions in it to install the update.

We have some reference designed based on DSC products, including 56F805, please look into this link:

http://www.freescale.com/webapp/sps/site/application.jsp?code=APLPMSYNCMO

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信