Hello All, I want to program DSP56F805 for PMSM, can somebody guide me how to start ? which version of codewarrior is suitable?, I will be using windows7 operating system.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello All, I want to program DSP56F805 for PMSM, can somebody guide me how to start ? which version of codewarrior is suitable?, I will be using windows7 operating system.

1,117 Views
chandankumar
Contributor I

I am good at "python" programming but new to "C/C++". Kindly suggest me best way to start with it.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,046 Views
TICS_Fiona
NXP Employee
NXP Employee

Hi CHANDAN,

Please use CodeWarrior v8.3 to develop for DSP56F805, which can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-56800E-DSC

It only supports C and assembly language.

CodeWarrior v8.3 can work on Windows 7. But to support USBTAP debugging on Windows 7, user needs to install the new CCS update, please search 'AN4338' on Freescale's website (www.freescale.com), and follow the instructions in it to install the update.

We have some reference designed based on DSC products, including 56F805, please look into this link:

http://www.freescale.com/webapp/sps/site/application.jsp?code=APLPMSYNCMO

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply