Hands on Workshop lab example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hands on Workshop lab example

2,261 Views
bjhwang
Contributor I

Hello there,

I would like to ask some questions about using this S12ZVMEVB(MTRCKTSBZVM128).

I searched some application notes(examples) to train and I found out pdf file about running BLDC motor using S12ZVM.

It is called hands on workshop: BLDC control using S12ZVM and while I was reading it, there were some lab example which I couldn't find on the website.
So my questions are.....

1. Is there any chance to receive these lab example to train?

2. If not, could you recommend basic sw to train?

Thanks for reading my poor English and I hope to hear some feedback soon :smileyhappy:

Thanks again

Tags (1)
0 Kudos
Reply
2 Replies

2,140 Views
jgerhardy
Contributor III

Hello ZhangJennie,

the document name is DWF13_AMF_AUT_T0526.pdf. It can be found on the NXP site here:

https://www.nxp.com/docs/en/supporting-information/DWF13_AMF_AUT_T0526.pdf 

I would also be interested (and maybe others as well) in the labs and example code for this workshop and

would appreciate any help you can give.

Regards,

John

0 Kudos
Reply

2,141 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi BJ,

To avoid misunderstanding, could you please send us the link of the document thus we can check it further?

Thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply