HELP! FreeMaster_SCI connection question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HELP! FreeMaster_SCI connection question

1,242 Views
_weh___george
Contributor I

HELP! FreeMaster_SCI connection question

 

I have build a FreeMaster_SCI code with PE, but have some question when I tried to connect the PC, and the error show "Can not detect the board information! The communication will be paused. Error code:0x80000101(Response timeout.)"

Thanks foe your help!

Labels (1)
0 Kudos
Reply
1 Reply

1,134 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello George

Which chip do you used ?

Do you used the UART to connect ? If yes, please check whether select the right one .

And there is a tutorial about how to use Freemaster  :

Tutorial: FreeMASTER Visualization and Run-Time Debugging | MCU on Eclipse  

Hope it heps

Alice

0 Kudos
Reply