HCS08 PWM DUTY PROBLEM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HCS08 PWM DUTY PROBLEM

6,760 次查看
venkateshgv
Contributor II

Hai,

 Am using  MC9S08SG8 micro controller ,and am using code warrior V6.3  software ,here am using PWM in 7th pin ,

 my problem is in  output duty cycle  first pulse is grater then the other pulse ,like this. plz any one can help me.

Capture.PNGThanks  in advance ,

Regards,

karthik

标签 (1)
0 项奖励
回复
7 回复数

6,512 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi karthik,

I am not familiar with S08 product.

Have you try to select the counter clock source after written duty cycle?

Best Regards,

Robin

0 项奖励
回复

6,512 次查看
venkateshgv
Contributor II

thanks a lot ,

 can u share a PWM example code, in coed warrior ,any micro controller

0 项奖励
回复

6,512 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Please check the following code

void main(void)
{
SOPT2 = SOPT2_T1CH1PS_MASK | SOPT2_T1CH0PS_MASK;
PTBDD_PTBDD6 = 1; //Pin as output
PTBD_PTBD6 = 0; // PTC1 in Low

PTCDD_PTCDD1 = 1; //Pin as output
PTCD_PTCD1 = 1; // PTC1 in High
// TPM clock = BUSCLK = 8MHz,channel operate in edge-aligned, Overflow Interrupt Enabled


TPM1SC = 0;

// Configure channel 1 High true pulses Edge aligned
TPM1C1SC = TPM1C1SC_ELS1B_MASK | TPM1C1SC_MS1B_MASK;
TPM1C1V = 4000; // channel 1 set to 50%

TPM1SC = TPM1SC_CLKSA_MASK | TPM1SC_TOIE_MASK;
TPM1MOD = 8000; // PWM frequency is about 1 KH

EnableInterrupts;

for(;;)
{
__RESET_WATCHDOG(); /* feeds the dog */


} /* loop forever */
/* please make sure that you never leave main */
}

/**************************************************************************************************/

void interrupt VectorNumber_Vtpm1ovf TPM1ovfISR (void)
{
//Clear interrupt flag
(void)TPM1SC;
TPM1SC_TOF = 0;
PTBD_PTBD6 ^= 1;


}

/**************************************************************************************************/

This is for the S08SH family

If you are using the external clock, maybe you are getting a different time on the first cycle due the clock set up.

I recommend you check the following document

https://www.nxp.com/docs/en/user-guide/HCS08QRUG.pdf 

I hope this will help

0 项奖励
回复

6,512 次查看
venkateshgv
Contributor II

Thanks a lot ,

 Am using the  software code warrior V6.3 , MC9S08SG8 8 pin package  type and here am attach my sample code ,

 this code i have a same problem above mention , 7th pin of controller is pwm am using internal clk. 

and this is my code .


/* Including needed modules to compile this module/procedure */
#include "Cpu.h"
#include "Events.h"
#include "PWM1.h"
/* Include shared modules, which are used for whole project */
#include "PE_Types.h"
#include "PE_Error.h"
#include "PE_Const.h"
#include "IO_Map.h"

unsigned int ADC_RESULT_TOTAL,ADC_RESULT[10],adc_value;
char a,b;
unsigned int ADC();
/* User includes (#include below this line is not maintained by Processor Expert) */

void main(void)
{
/* Write your local variable definition here */

/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
PE_low_level_init();
/*** End of Processor Expert internal initialization. ***/

/* Write your code here */
/* For example: for(;;) { } */
PWM1_Disable();
PWM1_ClrValue();
Cpu_Delay100US(1000);
for(;;)
{

setReg16(TPM2MOD, 4076);// period for 407Hz
TPM2C0V =3057; // 75% duty cycle
PWM1_Enable(); // enable the pwm
Cpu_Delay100US(5000); // delay for 50msec
PWM1_Disable(); // disable the pwm
Cpu_Delay100US(5000);

}


/*** Don't write any code pass this line, or it will be deleted during code generation. ***/
/*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/
for(;;){}
/*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/
} 

0 项奖励
回复

6,512 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

please test the code that I send you and tell me if you have the same problem with this code.

Thanks

6,512 次查看
venkateshgv
Contributor II

thanks for u r reply ,i try this code same problem has occuring.

Thanks

0 项奖励
回复

6,512 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

In my code, it starts in low, it takes a little bit more, due to the power on set up, but after that, all the pulse are the same

 pastedImage_2.png