FreeMASTER crash when configuring Packet Driven BDM communication plug-in

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeMASTER crash when configuring Packet Driven BDM communication plug-in

2,284件の閲覧回数
daniel_aciubota
Contributor I

FreeMASTER crashes when I try to configure the "FreeMASTER Packet Driven BDM Communication" Plug-in.

In the "BDM cable Settings" menu if I click a different option than the default one the program crashes (exits without any message). 

I have this issue using FreeMASTER versions 2.08, 2.09 and 1.4.4 on a system with OS Windows 10 Pro version 1803.

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,055件の閲覧回数
daniel_aciubota
Contributor I

The crash was caused by the debugger (P&E Micro) drivers.

An update of the drivers solved the issue.

(The USB Multilink driver version that works is 12.7.0.0 )

2,055件の閲覧回数
guenter_loettrich
NXP Employee
NXP Employee

Hi all,

in my case it seems to be related to the build of the used Windows 10 version.

Windows 10 Enterprise, Version 1709 works ok but version 1803 doesn't work.

0 件の賞賛
返信