Flash programmer for 56F8xx stand alone

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash programmer for 56F8xx stand alone

ソリューションへジャンプ
2,208件の閲覧回数
giamma
Contributor I

Qualcuno sa suggerirmi come programmare la flash dei DSP serie 56F8xx in Windows 7 con un software che non sia CodeWarrior

ラベル(1)
0 件の賞賛
返信
1 解決策
2,025件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Giovanni

The programming tools for 56F80x we supply include:

1)  CodeWarrior for DSP56800/E

2)  Flash_over_jtag

3)  Bootlader.

1) and 2) are both using JTAG interface. 3) uses SCI or CAN interface.

flash_over_jtag can only support parallel connection, it does not support USB interface. It does not support Windows 7 either.  I attached this tool.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,026件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Giovanni

The programming tools for 56F80x we supply include:

1)  CodeWarrior for DSP56800/E

2)  Flash_over_jtag

3)  Bootlader.

1) and 2) are both using JTAG interface. 3) uses SCI or CAN interface.

flash_over_jtag can only support parallel connection, it does not support USB interface. It does not support Windows 7 either.  I attached this tool.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,025件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

Translate with google:

    Suggest someone knows how to program the flash of the DSP series 56F8xx in Windows 7 with software that is not CodeWarrior

I think the answer will depend of the interface used ?

I've found some information on the web:

     DSP56F801|Digital Signal Controller|NXP

Interesting doc at:

     http://cache.nxp.com/files/product/doc/AN1926.pdf

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信