Flash programmer for 56F8xx stand alone

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash programmer for 56F8xx stand alone

Jump to solution
2,187 Views
giamma
Contributor I

Qualcuno sa suggerirmi come programmare la flash dei DSP serie 56F8xx in Windows 7 con un software che non sia CodeWarrior

Labels (1)
0 Kudos
Reply
1 Solution
2,004 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Giovanni

The programming tools for 56F80x we supply include:

1)  CodeWarrior for DSP56800/E

2)  Flash_over_jtag

3)  Bootlader.

1) and 2) are both using JTAG interface. 3) uses SCI or CAN interface.

flash_over_jtag can only support parallel connection, it does not support USB interface. It does not support Windows 7 either.  I attached this tool.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,005 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Giovanni

The programming tools for 56F80x we supply include:

1)  CodeWarrior for DSP56800/E

2)  Flash_over_jtag

3)  Bootlader.

1) and 2) are both using JTAG interface. 3) uses SCI or CAN interface.

flash_over_jtag can only support parallel connection, it does not support USB interface. It does not support Windows 7 either.  I attached this tool.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,004 Views
trytohelp
NXP Employee
NXP Employee

Hi,

Translate with google:

    Suggest someone knows how to program the flash of the DSP series 56F8xx in Windows 7 with software that is not CodeWarrior

I think the answer will depend of the interface used ?

I've found some information on the web:

     DSP56F801|Digital Signal Controller|NXP

Interesting doc at:

     http://cache.nxp.com/files/product/doc/AN1926.pdf

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply