Flash File to Target Problem with Kinetis E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash File to Target Problem with Kinetis E

3,464 Views
dhruvonline
Contributor III

Helllo,

 

I have developed a custom KE04Z8- 20pin SOIC based board. I am able to download and debug the program using Main Source Code Project.

But when i use the Flash File to Target option by browsing the Hex File, I am not able to download into the device. It is giving below errors. Please suggest. I am attaching screenshot for the same.

 

Regds,

Dhruv

Labels (1)
Tags (1)
3 Replies

3,257 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Dhruv ,

In addition, I would like to attach my video for how to use simple flash from my side.

hope this can also help.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,258 Views
BlackNight
NXP Employee
NXP Employee

Hello,

as noted in the error message of that dialog, you need to specify a target task name.

See that edit box at the bottom of the dialog: specify a name like

MyFlashToFile

or something like this.

I hope this helps,

Erich

0 Kudos
Reply

3,258 Views
dhruvonline
Contributor III

Hi,

Thanks for the response.

I have added the Task Name Also. See the error observed in the second page.

Regds,

Dhruv@ !@New Bitmap Image.bmp

0 Kudos
Reply