Failed to resume target process.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to resume target process.

4,644 Views
unclemike
Contributor III

I am getting the error "Failed to resume target process." from my debugger.  I am using CW 10.6 and a MC9S08QE32 chip

 

Things I have tried include:

 

Doing a 'clean'

Doing a 'regenerate processor expert" code.
deleted the .metadata folder.

tried to build in a different computer.

 

none of these things helped.

 

I CAN make a new project with processor expert, and it will debug just fine.

 

(I tried to upload a similar question a few hours ago, but I dont see it yet.  my apologies if this is redundant)

 

Thanks

Michael

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

4,195 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Micheal,

if there is no problem with a new project but problem is only in one specific project:

the possible reasons can be:

1. select wrong MCU type.

2. select wrong MCU connection

3. wrong memory definition in project

there is useful thread for similar problem, please see:

https://community.freescale.com/message/426740#426740

if you can't solve your problem anyway, please upload your project here we can test.

does this answer your question?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,195 Views
unclemike
Contributor III

Hi Jennie:

Thank you for responding.   On  the Processor Expert pane under "Generator Configurations" it has the wrong MCU in both projects that work and projects that don't.  I don't see where I select it when I am using the New Project wizard, and I can't find where to change it after the project has been created.  I select MC9S08QE32 when I am given a choice, but it seems to use whatever it fells like for the package suffix.  On the project that works under "Generator Configurations" it has "Debug_S08QE32CFT". On the project that does not work it has "S08QE32CWL.  The MCU is really a MC9S08QE23CLC,

On the Processor Expert pane under  Processors it has the correct MCU ( it says Cpu:MC9S08QE23CLC).  I can change that one by opening the hardware perspective and clicking on the "Select Package for the Processor" icon.

I have tried to select the correct MCU in the Components Library-> QE-> MC9S08QE32.  I double click on MC9S08QE32 and select the CLC package

I don't know if any of this has anything to do with my problem.  I was able to debug this project when I first made it.

I would upload my project, but I don't see an "add attachment" button here.  Where do I upload a file and how do I make sure that it goes to you instead of somebody else?

Mike

0 Kudos
Reply

4,191 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

your QE32 is CLC package so you need project mcu config as CLC package, right?

see attached for how to attach


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,191 Views
unclemike
Contributor III

Hi again:

This is the window I see.  there is no 'attach' in the lower right.

noattach.JPG.jpgH

However, since I can insert images, here is a shot of my screen.

package.JPG.jpg

Maybe it would be better if I took a different approach.  I am going to try to start a project from scratch and then see if I can find a way to move the Processor Expert files from the old project to the new one.  I was hoping  to avoid all those dialogs. 

You don't have to answer this if you don't want to.  Thank you for trying to help

Michael

0 Kudos
Reply

4,192 Views
unclemike
Contributor III

Hi Jennie:

Thank you for responding.   On  the Processor Expert pane under "Generator Configurations" it has the wrong MCU in both projects that work and projects that don't.  I don't see where I select it when I am using the New Project wizard, and I can't find where to change it after the project has been created.  I select MC9S08QE32 when I am given a choice, but it seems to use whatever it fells like for the package suffix.  On the project that works under "Generator Configurations" it has "Debug_S08QE32CFT". On the project that does not work it has "S08QE32CWL.  The MCU is really a MC9S08QE23CLC,

On the Processor Expert pane under  Processors it has the correct MCU ( it says Cpu:MC9S08QE23CLC).  I can change that one by opening the hardware perspective and clicking on the "Select Package for the Processor" icon.

I don't know if any of this has anything to do with my problem.  I was able to debug this project when I first made it.

Mike

0 Kudos
Reply