Failed to resume target process. Downloading binary to target

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to resume target process. Downloading binary to target

2,310件の閲覧回数
marionmees
Contributor I

I use a P&E CyclonePro with an adapter bord to program my MC9S08QD2 device. Reprogramming works but if I try to start the debugger I get the message "Failed to resume target process. Downloading binary to target..." Can anyone help me what could be the reason? 

I already tried to delete the .metadata and checked for overlapping of addresses but can't see the problem. 

0 件の賞賛
返信
2 返答(返信)

2,111件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Marion,

could you post your complete error message? E.g. it could be the one described in Please Check Your License | MCU on Eclipse .

Or it could be that you haver overlapping memory areas (see Problem Occurred: Flash programming with overlapping memory | MCU on Eclipse )?

Other than that, there is a checklist here: Debugging Failure: Check List and Hints | MCU on Eclipse 

I hope this helps,

Erich

0 件の賞賛
返信

2,111件の閲覧回数
marionmees
Contributor I

Hello Erich,

thanks for your fast response.

Finally in the target settings I used another connection configuration and

the debugger worked...

until now I didn't have the time to check for the difference which caused

the problem, I just use it as it is :smileywink:

Regards,

Marion

2018-03-07 16:16 GMT+01:00 BlackNight <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Failed to resume target process. Downloading binary to target

reply from Erich Styger

<https://community.nxp.com/people/BlackNight?et=watches.email.thread> in *CodeWarrior

Development Tools* - View the full discussion

<https://community.nxp.com/message/993192?commentID=993192&et=watches.email.thread#comment-993192>

0 件の賞賛
返信