Facing Link error L4025: This limited version allows only 32768 bytes of C code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Facing Link error L4025: This limited version allows only 32768 bytes of C code

2,650 Views
kshitijgupta
Contributor I

L4025: This limited version allows only 32768 bytes of C code

 

I am using Code Warrior IDE Version 5.9.0  Build 5294.

what can I do to minimize code size?

Please help me.

Labels (1)
0 Kudos
Reply
1 Reply

1,655 Views
trytohelp
NXP Employee
NXP Employee

Hi,

CodeWarrior IDE version 5.0.9 is the version of the IDE and not the tool version.

The IDE is a feature as the compiler, linker or debugger.

We need to know exactly the tool version used.

To do that you must:  Under CodeWarrior IDE (classic)

                Start the IDE and click on Help | About Freescale CodeWarrior.

                Click on Installed Products

                Provide us all info displayed.

                Or you can save them in a txt file.

If the Installed Products is not available for older version you should find information in the welcome.txt

under the installation folder.

Most of the time the tool is running at Special Edition level (Free of charge).

This is may be the version you're using.

Else do you have purchased another Suite (Basic, Standard or Professional) ?

See below some info regarding the Special Edition restrictions:

    CodeWarrior Development Tools Suite - Special|NXP

If you're using an older version, the code size could be reduced for special Edition.


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply