Error when using PE MICRO multilink with CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error when using PE MICRO multilink with CodeWarrior

1,491 Views
allenwong
Contributor II

Hello,


Anyone can help me on this?

 

INF: P&E Interface detected - Flash Version 6.15

ERR: Can not enter background mode  .

INF: Unable to initialize PEDebug.

GDI: => DI_ERR_NONFATAL GDI:

The Debugger can not connect to the P&E device

GDI: DiGdiClose()

GDI: => DI_OK

 

I try to program MK30DX256VLL7 customer's board and I got this error message.


Any idea to this?

 

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,432 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Allen,

- is this problem in a specific project or a common issue for all project?  how it work if you create a new project with wizard?

- remove .metadata folder in your current workspace then restart CW to test it again.

- do you use P&E multlink universal ?

- please follow this link to check your connection problem:

Debugging Failure: Check List and Hints | MCU on Eclipse


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply