Error starting with DEMO9S12xDT512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error starting with DEMO9S12xDT512

1,776 Views
mwendzao_oussei
Contributor I

Hello,

 

I’m trying to get start with DEMO9S12xDT512.

I downloaded evaluation license Code Warrior 5.2 in nxp website.

I also took the content of DVD of the demo.

First, when I try to build the project without doing anything it was missing mc9s12xdt512.h, I add it.

After that one build error was “XGVBR not declared” but I can see it on mc9s12xdt512.h.

The compiler does not see mc9s12xdt512.h but it can see XGVBR. I commented XGVBR the compilation was ok so the debug IDE opened, but some error appear, first was about P&E_ICD*.cmd after that the problem was mcu03f01.fpp the file is missing, Freescal directory I can find MCU03f(5,2,4,6).fpp but not the one. Where can I find it please?

Please, anyone can help me to get start with this DEMO.

 

Thank you in advance for your help

 

BR

0 Kudos
Reply
1 Reply

1,733 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI  Mwendzao OUSSEINE

I noticed you use mc9s12xdt512, however CW5.2 doesn't support this part. Please use CW5.1 instead.

Please note, CW5.1 can't work under windows 10


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply