Error found after trying to download program in to mpc5634m

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error found after trying to download program in to mpc5634m

跳至解决方案
1,257 次查看
mootan
Contributor II

I'm trying to download program using the program cw_progppcnexus.exe that you recommend but i encounter "Cannot enter background mode.

标签 (1)
1 解答
1,136 次查看
TICS_Fiona
NXP Employee
NXP Employee

Are you using TRK-MPC5634M? Or the board designed by yourself? Are you program with P&E USB multilink or OSJTAG?

For using TRK-MPC5634M, first, please check how the J1 and J5 jumpers are set on TRKMPC5604B. if SBC_5V is selected then J5 (Vsup) should be closed to enter SBC chip into debug state.

If the issue still exists, try to uninstall the P&E USB multilink or OSJTAG drivers, then reinstall it.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,137 次查看
TICS_Fiona
NXP Employee
NXP Employee

Are you using TRK-MPC5634M? Or the board designed by yourself? Are you program with P&E USB multilink or OSJTAG?

For using TRK-MPC5634M, first, please check how the J1 and J5 jumpers are set on TRKMPC5604B. if SBC_5V is selected then J5 (Vsup) should be closed to enter SBC chip into debug state.

If the issue still exists, try to uninstall the P&E USB multilink or OSJTAG drivers, then reinstall it.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------