Error found after trying to download program in to mpc5634m

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error found after trying to download program in to mpc5634m

ソリューションへジャンプ
1,271件の閲覧回数
mootan
Contributor II

I'm trying to download program using the program cw_progppcnexus.exe that you recommend but i encounter "Cannot enter background mode.

ラベル(1)
1 解決策
1,150件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Are you using TRK-MPC5634M? Or the board designed by yourself? Are you program with P&E USB multilink or OSJTAG?

For using TRK-MPC5634M, first, please check how the J1 and J5 jumpers are set on TRKMPC5604B. if SBC_5V is selected then J5 (Vsup) should be closed to enter SBC chip into debug state.

If the issue still exists, try to uninstall the P&E USB multilink or OSJTAG drivers, then reinstall it.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,151件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Are you using TRK-MPC5634M? Or the board designed by yourself? Are you program with P&E USB multilink or OSJTAG?

For using TRK-MPC5634M, first, please check how the J1 and J5 jumpers are set on TRKMPC5604B. if SBC_5V is selected then J5 (Vsup) should be closed to enter SBC chip into debug state.

If the issue still exists, try to uninstall the P&E USB multilink or OSJTAG drivers, then reinstall it.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------