Error: Code Warrior 10.6 and java.lang.Boolean

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error: Code Warrior 10.6 and java.lang.Boolean

1,466 Views
kappa74
Contributor IV

Good morning,

my PC has Windows 8. I installed MQX10.6.

When I import the project bsp_twrmcf5259, I'll get the error: CW ProjectView Project Loading Verification: An internal error has occurred: java.lang.Boolean cannot be cast to java.util.List.

I wanto to say that  iused for all day the CW10.6 in Windows 8 but in the evening appears this error and  I can't work.

Have you any idea?

 

13737_13737.jpgJava_error.jpg

 

Best Regards

Mirko

Labels (1)
0 Kudos
Reply
1 Reply

1,279 Views
trytohelp
NXP Employee
NXP Employee

Hi Mirko,

Same problem reported to the SR 1-2156305851.

I've checked 2 win 8 32 and 64 bit configurations:

      - java 7 update 67,

      - MCU v10.6,

      - MQX v4.1.

I can open the \Freescale_MQX_4_1\build\twrmcf52259\cw10\build_libs.wsd and build all libs without problem.

To check it, I've created an example for twrmcf52259 through the wizard for hello project.

I can build this project too.

Is there a problem with Java or Freescale installation ?

I recommend you to unisntall and re-install Java and Freescale tool.

I've checked in our data base and under google and don't find interesting post regarding this error.

May be other community members could provide you other hints.


Have a great day,
Pascal Irrle

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply