Error 41 During script

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error 41 During script

4,470 Views
vijaysrinivasa
Contributor II

I am working on TRK - MPC5606B Starte TRAK Development Board , code warrior IDE version 5.9.0 and P&E debugger USM-ML-PPCNEXUS.

 

I have taken the example code for SWvector  from installation holder (C:\Program Files (x86)\Freescale\CW for MPC55xx and MPC56xx 2.6\(CodeWarrior_Examples)\560xB-CW\INTC-SWvector-VLE )

 

Make is happening and when try to debug , getting  Error 41 below is the message

Getting the Error message Like

 

Error: Error in ONCE Status register during instruction excution.

Error: Error in ONCE Status register during instruction excution.

Error: Error in ONCE Status register during instruction excution.

-

-

-

 

RAM>; Automatically generated script file for PPCNEXUS Flash Programming

CMD>CM c:/program file(x86)\freescale\cw for mpc55xx and mpc56xx 2.6\pemicro\algorithms\000000

 

Error 41 during the script

.pcp file does not exist

 

how to get the .pcp file 

Can any one help me how to resolve this issue

 

Best regards

vijay

Labels (1)
5 Replies

4,282 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

Have you correctly installed PEMicro drivers?

Are you able to download the code to flash or RAM memory?

Could you please send me a step-by-step process how you download the code to microcontroller and how you try debug it?

Regards,

Martin

4,282 Views
vijaysrinivasa
Contributor II

Hello Martin kovar

Thank you for your reply , as you said there was a patch file missing for PEMicro divers , i have got from P&E team.

Now it is working. able to download and debug

Best regards

vijay

4,282 Views
lishaoming
Contributor II

Hi, I met the same problem. Where can I find the patch file?

0 Kudos
Reply

4,282 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

please check pemicro website, or contact pemicro support directly.

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 

Regards,

Martin

4,282 Views
lishaoming
Contributor II

Thank you, I have get it.

0 Kudos
Reply