Enquiry on processor MPC5200

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enquiry on processor MPC5200

8,173 次查看
evanlim
Contributor I

Hi,

 

Is their any other hardware that I can use to do flash programming and hardware Dianosigic with MPC5200 PowerPC e300 Core Integrated Processor (400MHz)?

 

I had tried with Codewarrior Tap CWH-CTP-BASE-HE but the CodeWarrior doesn't seems to connect to my target board.

I tried using CWH-UTP-PPCD-HE and i can perform flash programming as well as hardware Dianosigic.

 

Thanks.

 

Regards,

Evan

标签 (1)
0 项奖励
回复
6 回复数

8,035 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Evan

The part number of USBTAP that support MPC5200 is CWH-UTP-PPCC-HE. However it is not manufactured now.

Its replacement is CWH-CTP-BASE-HE.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW_TAP

However if you are using CodeWarrior for MobileGT v9.2, you need install CCS update. For details, please review this document:

http://cache.freescale.com/files/32bit/doc/app_note/AN4780.pdf

CodeWarrior for MobileGT v9.2 also supports Abatron BDM-2000.  In CodeWarrior's Connection select menu,  the connection name for it  is Abatron Serial and Abatron TCP/IP.

Hope it helps!

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

8,031 次查看
evanlim
Contributor I

Hi Fiona,

Can I have a list of CodeWarrior that can support MPC5200?

From the previous version(older version) till current.

Thanks.

Regards,

Evan

0 项奖励
回复

8,031 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Evan

The latest CodeWarrior version that supports MPC5200 is v9.2:

CodeWarrior Development Tools for mobileGT|NXP

MPC5200 is an old product, and we have not updated its CodeWarrior for many years.

Best Regards

Fiona Kuang

TIC - Technical Information Center

0 项奖励
回复

8,031 次查看
evanlim
Contributor I

Hi Fiona,

Sorry, I’m referring to the Codewarrior USB TAP.

Would like to know what other Codewarrior USB TAP supports MPC5200.

Thanks.

Regards,

Evan

0 项奖励
回复

8,031 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Evan

The part number was included in my first reply.

The part number of USBTAP that support MPC5200 is CWH-UTP-PPCC-HE. However it is not manufactured now.

Its replacement is CWH-CTP-BASE-HE.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW_TAP

Best Regards

Fiona Kuang

TIC - Technical Information Center

0 项奖励
回复

8,031 次查看
evanlim
Contributor I

Hi Fiona,

CWH-UTP-PPCC-HE is the only Codewarrior USB TAP that can support MPC5200? There’s no other version or previous version that can support MPC5200?

And CWH-CTP-BASE-HE is the only replacement that we can use with MPC5200?

Currently we could not use CWH-CTP-BASE-HE to test out our target board.

We tried with CWH-UTP-PPCC-HE and can be tested.

But we could not get any CWH-UTP-PPCC-HE as it is not manufactured now.

We would like to know the list of Codewarrior USB TAP that can support MPC5200 so that we can have more option to source for.

Thanks.

Regards,

Evan

0 项奖励
回复