Enquiry on Codewarrior TAP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enquiry on Codewarrior TAP

6,954件の閲覧回数
evanlim
Contributor I

Hi,

 

Would like to check can Codewarrior TAP CWH-UTP-PPCD-HE supports MPC5200?

If not, what other Codewarrior TAP can i use?

To do flash programming.

 

Thanks.

 

Regards,

Evan

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

6,782件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Evan

The part number of USBTAP that support MPC5200 is CWH-UTP-PPCC-HE. However it is not manufactured now.

Its replacement is CWH-CTP-BASE-HE.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW_TAP

If you are using CodeWarrior for MobileGT v9.2, you need install CCS update. For details, please review this document:

http://cache.freescale.com/files/32bit/doc/app_note/AN4780.pdf

Hope it helps!

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,779件の閲覧回数
evanlim
Contributor I

Hi,

I’m reading through the CW user guide and try to connect the CW using Lan cable. But I don't really understand.

Where can I find the "netparam" and "core" ? (See attached file)

Check with you, the IP Address for my CW is 192.168.3.255 ? (See attached file “CCS – IP address”)

Thanks.

Regards,

0 件の賞賛
返信

6,779件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Evan

CodeWarrior TAP can be connected with either Ethernet interface or USB interface. 

When connect with Ethernet interface, please select Ethernet TAP when create the new connection in CodeWarrior for MobileGT v9.2, and in the hostname field, enter the IP address of the CWTAP, or fsl<last digits of the CWTAP MAC address>.

For details, please refer to:

http://cache.freescale.com/files/32bit/doc/app_note/AN4780.pdf

 

Regarding to your question about CodeWarrior TAP set up utility, please open the telnet session and connect to the CodeWarrior TAP probe by: telnet hostname.

For details, please refer to section 6.1 in CodeWarrior TAP Probe User Guide. 

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 件の賞賛
返信