ERROR :    C5200 : xxx.h file not found

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ERROR :    C5200 : xxx.h file not found

5,212件の閲覧回数
azeddinehaida
Contributor I

Hi,

I'm using CW 6.3 in windows xp and I've tried to compile my HCS08 project but i had this tipe of ERROR for many files.h which i'm sure they were in code folder (when i clicked on compile the files.h are deleted).

 

Thank you in advance

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

4,538件の閲覧回数
azeddinehaida
Contributor I

Hi,

thank you very much I solved it unistalling and installing CW.

-The specific xxx.h file was included in the project and specified correctly

0 件の賞賛
返信

4,538件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

good to know.. Thanks for sharing your solutions here!

0 件の賞賛
返信

4,538件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI,

Normally ERROR : C5200 : xxx.h file not found

Is because:

  • - The specific xxx.h file isn’t included in the project, please perform search in your project folder for this file. Can you search it out?

Or

  • - The path or name of the xxx.h file isn’t specified correct. Please check the path setting of it.

Can you solve your problem with above hint? If not, please upload your project here. I will check problem directly from my side. Thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信