ERROR :    C5200 : xxx.h file not found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ERROR :    C5200 : xxx.h file not found

5,181 Views
azeddinehaida
Contributor I

Hi,

I'm using CW 6.3 in windows xp and I've tried to compile my HCS08 project but i had this tipe of ERROR for many files.h which i'm sure they were in code folder (when i clicked on compile the files.h are deleted).

 

Thank you in advance

Labels (1)
0 Kudos
Reply
3 Replies

4,507 Views
azeddinehaida
Contributor I

Hi,

thank you very much I solved it unistalling and installing CW.

-The specific xxx.h file was included in the project and specified correctly

0 Kudos
Reply

4,507 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

good to know.. Thanks for sharing your solutions here!

0 Kudos
Reply

4,507 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI,

Normally ERROR : C5200 : xxx.h file not found

Is because:

  • - The specific xxx.h file isn’t included in the project, please perform search in your project folder for this file. Can you search it out?

Or

  • - The path or name of the xxx.h file isn’t specified correct. Please check the path setting of it.

Can you solve your problem with above hint? If not, please upload your project here. I will check problem directly from my side. Thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply