EQADC reference voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EQADC reference voltage

2,718件の閲覧回数
pier-luc_rosa
Contributor II

In the spec it says we can select 1.25V 2.5V or 5V as voltage reference. Is this only possible by manually changing reference voltage on the pin ? Or is it possible to select an internal reference voltage?

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,705件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Well, it is hard to comment, as you did not shared which device you are referring to.

Best regards,

Peter

0 件の賞賛
返信

2,700件の閲覧回数
pier-luc_rosa
Contributor II

MPC5674F

0 件の賞賛
返信

2,674件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

For eQADC you can only have 5V reference.

VRH must be same as VDDA, and VDDA is 5V.

Best regards,

Peter

0 件の賞賛
返信