EQADC reference voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EQADC reference voltage

2,679 Views
pier-luc_rosa
Contributor II

In the spec it says we can select 1.25V 2.5V or 5V as voltage reference. Is this only possible by manually changing reference voltage on the pin ? Or is it possible to select an internal reference voltage?

Tags (1)
0 Kudos
Reply
3 Replies

2,666 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Well, it is hard to comment, as you did not shared which device you are referring to.

Best regards,

Peter

0 Kudos
Reply

2,661 Views
pier-luc_rosa
Contributor II

MPC5674F

0 Kudos
Reply

2,635 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

For eQADC you can only have 5V reference.

VRH must be same as VDDA, and VDDA is 5V.

Best regards,

Peter

0 Kudos
Reply