Does CodeWarrior have any API to set soft breakpoints directly?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does CodeWarrior have any API to set soft breakpoints directly?

ソリューションへジャンプ
2,509件の閲覧回数
blackmouse
Contributor I

I use the CodeWarrior 5.9.0. When I set a soft breakpoint then check the CCS log, only find these "ccs_read_reg" "ccs_write_reg" "ccs_write_mem" and some other APIs viewing memories or registers directly. So I want to know if there are some APIs to set soft breakpoints directly.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,407件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello customer,

No, these two functions are for hardware breakpoints. The software breakpoints works in different ways.

When software breakpoints are used, the debugger will remove the instruction and replace it with a special debug halt instruction into program Flash memory.   After the CPU starts running, periodically, the debugger polls the target for status to see if it has halted.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,407件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello customer:

Below are the CCS API functions for breakpoint set and remove:

ccs_error ccs_set_hwbp(ccs_core_handle coreh, unsigned long bp_info_size, void *bp_info, unsigned long reservation_id, unsigned long *bp_id);

ccs_error ccs_delete_hwbp(ccs_core_handle coreh, unsigned long bp_id);

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,407件の閲覧回数
blackmouse
Contributor I

But according to the help document they are hardware breakpoint APIs. Are they suitable for software breakpoints?

0 件の賞賛
返信
2,408件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello customer,

No, these two functions are for hardware breakpoints. The software breakpoints works in different ways.

When software breakpoints are used, the debugger will remove the instruction and replace it with a special debug halt instruction into program Flash memory.   After the CPU starts running, periodically, the debugger polls the target for status to see if it has halted.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信