Does CodeWarrior TAP support MPC8641D COP Interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does CodeWarrior TAP support MPC8641D COP Interface?

Jump to solution
2,081 Views
adrian_creegan
Contributor I

Hello All,

I have a few non-functioning MPC8641D powered boards with COP headers that need to be triaged.  It is not clear whether the processors are damaged or if the NVRAM content has been erased / corrupted.

I was wondering if the CodeWarrior TAP (CWH-CTP-BASE-HE) with an appropriate adapter (CWH-CTP-COP-YE) would be appropriate (mainly to examine the processor and NVRAM and maybe re-initialize NVRAM by copying from a working board)?  The CodeWarrior TAP does not list the MCP8641D processor as supported but questions in this forum seem to suggest that it is.  Is this the case?

Thanks in advance and kind regards,

Adrian.

Tags (2)
0 Kudos
Reply
1 Solution
2,007 Views
Pavel
NXP Employee
NXP Employee

Use CodeWarrior 8.8 for the MPC8641:

Install CodeWarrior and install CodeWarrior 8.8.6 patch for CodeWarrior TAP using.

This CodeWarrior is available using the following page:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
2,008 Views
Pavel
NXP Employee
NXP Employee

Use CodeWarrior 8.8 for the MPC8641:

Install CodeWarrior and install CodeWarrior 8.8.6 patch for CodeWarrior TAP using.

This CodeWarrior is available using the following page:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------