Does CW support an old 9S08QE8CWL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does CW support an old 9S08QE8CWL?

1,840件の閲覧回数
randenewberry
Contributor IV

I have CW10.6, and need to modify a "WL" package (28 pin SOIC). The only options in CW are for a LC or FM.

If I need to upgrade or pay a new license, I will.

Any help will be greatly appreciated.

ラベル(1)
0 件の賞賛
返信
1 返信

1,793件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Rande Newberry

I checked CW10.6, It can support 9S08QE8CWL, see attached video.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信