Differential ADC problem after updating CW 10.6 UPDATE 1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Differential ADC problem after updating CW 10.6 UPDATE 1

1,589件の閲覧回数
marco76
Contributor III

Today CW 10.6 required me to perform the automatic update named: UPDATE 1.

After that i've the following message when Processor Expert try to generating the project code that until now worked:

 

ERROR: Unexpected status of script: Drivers\56800\ADC_803x.ts2, please contact Freescale support

 

The project is based on MC56F84789 and the error is localized on one of the three ADC bean that i used.

 

I have found that this bean use a channel in differential mode. If i try to disable the differential mode the Processor Expert code generation is successful!

 

Does anyone have the same problem?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,352件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

I reproduced the problem on CodeWarrior v10.6. This should be a bug in PE and I have reported it to our development team as issue 45327962.  I will keep you informed for this problem fix.

0 件の賞賛
返信

1,352件の閲覧回数
marco76
Contributor III

Ok, thanks!

I reinstalled CodeWarrior v10.6 without the UPDATE 1.

I await a patch to fix the problem before doing the update again.

0 件の賞賛
返信

1,352件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

please find attached the hotfix for the problem for CW10.6.1.

We apologize for the inconvenience.

Best regards

Petr Hradsky

Processor Expert Support Team

0 件の賞賛
返信