Debug Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debug Error

2,050 次查看
fatihtaskincan
Contributor I

I have encountered an errors while applying the debug configuration which is showed as "An error has occurred. See error log for more details. The function "close" returned an error condition  (0x80004005) ". How can I able to this problem? By the way, solutions which have already exist in your forums didn't help me.

标签 (1)
0 项奖励
回复
3 回复数

1,933 次查看
TICS_Fiona
NXP Employee
NXP Employee

Thanks a lot for contacting us.

Would you please first create a new project for your MCU from <File> menu -> New->Bareboard project, can CodeWarrior program with this project into your board? If yes, please compare its options in <Run/Debug Settings> with your project.

If the new bareboard project also does not work, please reply with your CodeWarrior version and the part number of your MCU.  What’s the OS on your PC, is it a 32bit, or 64bit OS?

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,933 次查看
fatihtaskincan
Contributor I

On my PC there is a 64 bit operating system. The version of the my CodeWarrior is 10.6. I ve a TWR-56F8200 Tower System (motor control board) which contain MC56F82748 digital signal controller. I ve just tried to your example codes with helping a provided video,but it persistently gives the same error (0x80004005).

Thanks for reply. 

0 项奖励
回复

1,933 次查看
addiyi
NXP Employee
NXP Employee

Could you please provide more details about what version of CodeWarrior you are using and about your board/cpu?

Adrian

0 项奖励
回复