Debug Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug Error

1,952件の閲覧回数
fatihtaskincan
Contributor I

I have encountered an errors while applying the debug configuration which is showed as "An error has occurred. See error log for more details. The function "close" returned an error condition  (0x80004005) ". How can I able to this problem? By the way, solutions which have already exist in your forums didn't help me.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,835件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Thanks a lot for contacting us.

Would you please first create a new project for your MCU from <File> menu -> New->Bareboard project, can CodeWarrior program with this project into your board? If yes, please compare its options in <Run/Debug Settings> with your project.

If the new bareboard project also does not work, please reply with your CodeWarrior version and the part number of your MCU.  Whats the OS on your PC, is it a 32bit, or 64bit OS?

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,835件の閲覧回数
fatihtaskincan
Contributor I

On my PC there is a 64 bit operating system. The version of the my CodeWarrior is 10.6. I ve a TWR-56F8200 Tower System (motor control board) which contain MC56F82748 digital signal controller. I ve just tried to your example codes with helping a provided video,but it persistently gives the same error (0x80004005).

Thanks for reply. 

0 件の賞賛
返信

1,835件の閲覧回数
addiyi
NXP Employee
NXP Employee

Could you please provide more details about what version of CodeWarrior you are using and about your board/cpu?

Adrian

0 件の賞賛
返信