DSP56F805FV80E copy the program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSP56F805FV80E copy the program

1,463 Views
yersr71
Contributor I

I need to make a copy of the working chip program that would be transferred to another chip. With CodeWarrior Development Studio for 56800 / E Digital 8.3 (Windows 7), I want to save - Menu "Debug" -> "DSP56800" -> "Load / Save Memory". Specify the memory type, start address, size, destination filename, and file format (S-rec ...). Question-What start address and what file size should I specify for P and X memory, if I see data size larger than those specified in the data shirt when viewing the memory?

Tags (1)
0 Kudos
Reply
1 Reply

1,342 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Yury,

Regarding your questions, you can use the debugger features to save the data in memory into a file in binary or text with S19 format. You can use any file name, but the extension name should match with the data format. The start address can be any value, I am not sure the maximum size you can transfer, you have to try.

Hope it can help you

BR

Xiangjun rong