Creating a project form scratch problem (K20 - K10)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Creating a project form scratch problem (K20 - K10)

3,429件の閲覧回数
jamesalexander
Contributor I

Hi, I'm working with CW10.3 and FRDM-K20D50M.

I`ve used the examples in both Baremetal kinetis_50mhz_sc.zip as PEX.

My intention is not to use the PEX.

When I create a new project using make_new_cw_project.exe everything works fine but if I start a project from scratch I can`t build it.

Suppose you use the make_new_cw_project.exe ..  can I migrate that code to a MK10D? Driver code included in kinetis_50mhz_sc.zip can be used with MK10D?

 

 

Thanks

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,309件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello FD,

- Do you use the MK10D 50M chip, if yes, you can migrate that code to a MK10D chip.

pastedImage_0.png

- "if I start a project from scratch I can`t build it." , if you want solve this problem ,

could you please give me a screenshot about this , or screenshot tell me how to reproduce the problem, i can test it on my side .

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------


Have a great day,
Alice Yang

0 件の賞賛
返信

3,305件の閲覧回数
jamesalexander
Contributor I

Hi, thanks for answer my question.

I`m currently using an FDRM-K20D50 board but in a short time i'll migrate

to my own custom hardware and it will have mounted a MK10

I built a code based on "Using the Freescale Header Files and Blinking the

LED" from https://community.freescale.com/docs/DOC-93960

This code written by Eli Hughes is runnig for a KL25 (m0+) so i create a

new BareBoard project for MK20DX128***5 without Pex. I use the same file

structure and main.c.

The error messages are :

..Workspace_II/common/common.h:36:4: error: #error "No valid platform

defined"

..Workspace_II/common/common.h:60:4: error: #error "No valid CPU defined"

..Workspace_II/common/common.h:71:19: fatal error: gnu.h: No such file or

directory

I belive that is a eclipse config problem , i tried a lot and i cant make

it work

I attached the project and a snapshot of the console

Thanks

On Wed, Dec 16, 2015 at 1:09 AM, Alice_Yang <[email protected]>

0 件の賞賛
返信

3,304件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

- You project have error when build on my side , i refer to the error changed some place .

And it now can build and debug well on FRDMK20D50 board ,please check the attachemtn .

- while i find you have not  change the pins to the board corresponding ,it still the configuration of FRDM-KL25, you need

configure it .

Hope it helps

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Have a great day,
Alice Yang

0 件の賞賛
返信