Create a new S12ZVM project in CW 11.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Create a new S12ZVM project in CW 11.0

984 次查看
hsg000
Contributor I

Now the Create a new S12ZVMC128 project in CW 11.0,When choosing the connected emulator again, I only chose P & E USB MultiLink, not Open Source BDM.

But now I have an OSBDM emulator, and since I do not choose Open Source BDM to connect, I can only download the program with the OSBDM emulator, not debug (cannot interrupt points, view variables, etc.)

If I select both connections when building a new project, you can do debug with OSBDM. So I want to ask you how to add a Open Source BDM connection option in an already existing project.

 

0 项奖励
回复
2 回复数

951 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Normally  P & E USB MultiLink launch configuration can also connect Open Source BDM interface.

If we need to create a new Open Source BDM manually, please

1. create a new project including Open source BDM launch configuration. Make sure we can connect board with this interface.

2. In your application, we create a new  set Debug configurations as below:

ZhangJennie_0-1704271599222.png

3. then create a new launch configuration, configure this launch configuration with referring the Open source BDM launch configuration in step 1

ZhangJennie_1-1704272508514.png

 

Hope this helps

Jun Zhang

 

 

0 项奖励
回复

978 次查看
hsg000
Contributor I

 

填充图片

hsg000_0-1704188092365.png

 

0 项奖励
回复