Component Development Tools Troubleshooting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Component Development Tools Troubleshooting

2,886件の閲覧回数
marceli1
Contributor III

Why can not import PEx component with driver *.drv to develop. It happens in CodeWarrior 11.1 and MCUXpresso. Also inherited component is not available in MCUXpresso, and in CodeWarrior  imported component is RO.

Regards,

Marceli

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,846件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Marceli Firlej,

processor expert is only supported in CodeWarrior.

MCUXpresso IDE doesn't support processor expert, and there is no plan to support it.

For MCUXpresso IDE, our recommended config tool is "MCUXpresso Config Tool" which is integrated in MCUXpresso IDE already. its standalone version is in this url

MCUXpresso Config Tools|Software Development for NXP Microcontrollers (MCUs) | NXP 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,846件の閲覧回数
marceli1
Contributor III

Processor Express is user language, which I can fast reconfigure mine application, not spending much time. Therefore I am using Code Warrior or Kinetis IDE. I also tried put PEx plugins to MCUxpresso but is not supporting toolchain properly, because Config Tool is not the same.

Thanks,

Marceli

0 件の賞賛
返信

2,846件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

MCUxpresso doesn't support PEx plugin.

0 件の賞賛
返信