Compilation Error in porting CW v6.3 project to CW v10.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compilation Error in porting CW v6.3 project to CW v10.6

1,434 Views
harshitbhimani
Contributor I

Hi , I am porting facing compiling error while porting project from CW v6.3 to v10.6.

The error is 

1.  "mingw32-make:***[Sources/XXX_c.obj] Error1.

2."mingw32-make:***Waiting for ufinished jobs....

Labels (1)
0 Kudos
Reply
1 Reply

1,321 Views
trytohelp
NXP Employee
NXP Employee

Hi,

Depending of your project, it could be less or more difficult to move the classic application to Eclipse.

I recommend you to refer to the AN4727:

AN4727, Import project from CW classic to CW MCU v10 4 CodeWarrior for Microcontrollers v10.4

                        http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf

For the error you reported, please click on Console Tab to get more information on the problem.


Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply