Codewarrior6.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior6.3

1,649 Views
as5818956
Contributor I
  • Codewarrior IDE 6.3 cannot open,"The IDE failure to start suggests that the IDE COM conponents are not registered properly.Run regservers.bat which is found in the same locaition as the IDE.exe program to register the components"

      cannot open the Codewarrior, have tried to  uninstall and install again,     but it just didn't work

0 Kudos
Reply
1 Reply

1,340 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI,

Try to run {CW 6.3 install folder}\bin\regservers.bat. Then restart CW.

If this can't work, please try reinstall CW package.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply